Technical features and installation information for the Spelsberg Wallbox

The Spelsberg Wallbox is the timeless charging station for electric cars, combining design and technology that impress in every respect. With its minimalist design the Wallbox blends stylishly into its installation environment, and the many features make every tech enthusiast's heart beat faster.

Safe and smooth connection of the Wallbox is particularly important. That's why we designed the Wallbox to be as easy to install as possible – you can find information about setting up the charging station for electric cars on this page. We have also compiled everything you need to know about the Wallbox's features. At the end of the page, you'll find a direct way to contact us.

The Spelsberg charging station – thoughtfully designed

Easy installation of the Wallbox

Designed for quick and easy commissioning, the Spelsberg EV charging station can be installed in just a few simple steps. Skilled installers can complete all installation steps efficiently, from alignment to wiring.

The Wallbox can be mounted and installed in just a few simple steps

The generous installation space gives the installer enough room to connect all cables effortlessly. The Wallbox enclosure also has numerous knockouts for cable insertion at the top, bottom and rear. This enables flexible cable routing.

Double membrane seals have also been pre-installed. The Enclosure cover is fitted with quick-release screws for quick opening and closing of the enclosure. The sliding mechanism allows the design cover to be easily slid into place and locked.

Finally, the Wallbox can be quickly and easily mounted on the house wall – the mounting rail and Drilling template make installation easier.

Convenient configuration via the Spelsberg app

The Wallbox can be easily connected to your home internet, either via Wi-Fi or an Ethernet cable. The final configuration of the Wallbox is completed via the Spelsberg Wallbox app. The installer therefore only needs a smartphone to commission the charging station at home.

Communication, interfaces and updates

The Spelsberg Wallbox is a communication expert: It can be effortlessly integrated into your home network via Wi-Fi or an Ethernet cable. With free over-the-air updates, the Wallbox keeps itself up to date and expands its range of functions.

The Spelsberg Wallbox can also communicate with energy management systems or external backend systems via OCPP 1.6, Modbus TCP and EEBus. Depending on requirements, the Wallbox can be configured with various extensions: for example, software for intelligent charging or cloud-based management software for charging stations, making electric-vehicle charging even more efficient.

You can find a detailed list of our partners here.

Compatibility with numerous partner systems

The Spelsberg Wallbox is more than just a charging station. It can be connected to numerous other systems and offers end customers maximum compatibility. Depending on requirements, the Wallbox can be configured with various extensions: for example, software for intelligent charging or cloud-based management software for charging stations, making electric-vehicle charging even more efficient.

You can find a detailed list of our partners here.

Authorisation to use the EV charging station

One person pays while everyone else uses the charging station? No, that is definitely not how it should be. Integrated authorisation protects against “energy theft.” Permission to use the charging station for electric cars is granted either by the electric vehicle itself (Plug & Charge and AutoCharge) or via an RFID chip.

This is particularly interesting for apartment buildings. Only authorised persons can access the charging station there. Evaluation can also be filtered by authorisation.

Load and charging management for the EV charging station

For those who need to monitor not just one charging station but manage an entire fleet, dynamic load management is available.

This means that up to 250 charging stations for electric cars can communicate with one another. A major advantage is that outages during peak loads are avoided and the available power is fully utilised.

If a vehicle is to be prioritised, that is no problem. You can decide which electric vehicle should be charged first at the charging station.

Control the EV charging station via the app

Complete management of the Wallbox is handled via the app. Simply pick up your smartphone and start a charging session or commissioning. The Spelsberg Wallbox gives you full control of the EV charging station at a glance. This provides an overview of consumption, charging duration, charging power and the current Wallbox status. The app is intuitive, easy and convenient to use.

Control, evaluate and bill charging station usage

For sustainable monitoring, the charging station contains an integrated MID-compliant meter. This meter displays, for example, the number of charging sessions, charging duration and energy charged for all sessions. Down to the user level (authorisation), it is possible to track who operated the charging station and when the electric vehicle was charged. For employees or self-employed users, this has the advantage that the energy charged by a company car can be billed.

Colors

Spelsberg Wallbox Smart Pro

The Wallbox Smart Pro expands its unique design with additional professional features.

  • All features for easy charging
  • Dynamic load management
  • Control and evaluation via app
  • Plug&Charge, AutoCharge
  • Integrated MID-compliant meter for consumption billing
  • Solar powered charging
  • Over-the-air updates in the background
  • Communication: Modbus, EEBus, SEMP

To the Spelsberg Wallbox Smart Pro

Your request